T
- Temper:
(1)The hardness and strength produced by mechanical or thermal treatment or both. It is characterized by a certain structure, mechanical properties or reduction in area during cold working. (2)A measurement of the degree of hardness or lack of ductility in a metal.
- Temperature Rating:
The maximum temperature at which a material may be used in continuous operation without a loss of its basic properties.
- Threaded Coupling:
A means of coupling mating connectors by engaging threads in a coupling ring with threads on a receptacle shell.
- Tight Buffer (Fiber Optic):
A material surrounding a fiber in a cable, holding it firmly in place.
- Tinning:
Coating of a terminal, lead or conductive pattern with tin or solder alloy to improve or maintain solderability or to aid in the soldering operation.
- Total Internal Reflection (Fiber Optic):
The phenomenon of light rays reflecting at the core-clad boundary of an optical fiber, allowing transmission along the length of the fiber. It occurs when the angle of incidence is lower than the critical angle.
- Transceiver:
A device that combines both a transmitter and a receiver.
- Transmission:
The transfer of electric energy from one location to another through conductors or by radiation or induction fields.
- Triaxial:
Refers to a three conductor cable with one conductor in the center, a second circular conductor shield concentric with the first, and the third circular conductor shield insulated from and concentric with the first and second, usually with insulation.
- Tubing:
A tube of extruded non-supported material.
- Twisted Pair:
A pair of wires twisted together, usually standard low-speed communications wire cables.