2016-05-09
LEMO receives Directindustry i-NOVO awards at Hannover Messe
During Hanover Messe 2016, LEMO participated in the Directindustry i-NOVO awards. Out of 25 nominees, two LEMO products got 1st and 3rd place in the Design and Tech categories respectively.
The Nicoral corrosion resistance received third place in i-NOVO Tech category and the IAC- Intelligent Active Connector received first place in the Design category.
The Nicoral surface treatment was first announced in July 2015 and has been generating a lot of interest for companies searching for MIL-spec like connectors. "The Nicoral surface tratment, allowing up to 500 Hours of salt spray corrosion on aluminium connectors is a great new corrosion treatment unlike existing products on the market", says Mathieu Menet the person behind the innovation.
The IAC - Intelligent Active Connector is a new range of connectors launched by LEMO a few weeks prior to the show. The Halo LED connector is a connector with a LED lighted flange allowing to display the connector status, thus enabling the user or operator to have an immediate visual indication of the connection status. When multiple connections need to be made, the user will know straight away if all the connexion setup is running fine.