Environment

Environmental considerations play an increasing role in driving business activities. LEMO complies with the ISO 14001 standard, the main European laws and regulations such as RoHS and REACH, as well as meeting the highest specific customer requirements.

Our environmental management system is ISO 14001 certified, which demonstrates LEMO's commitment to sustainable development and business practices. Our main objective is to limit the impacts of our activities on the environment by polluting less and consuming better. To reach this objective, LEMO performs a regular analysis of its environmental impacts and takes initiatives to reduce the most significant ones.
Product Conformity
LEMO ensures the continuous respect and conformity of the different regulations
RoHS
EU RoHS Directive refers to the restriction of the use of certain hazardous substances in electrical and electronic equipment (EEE), including connectors. LEMO certifies that connectors and accessories produced and supplied under the brands LEMO, REDEL and COELVER are compliant with 2011/65/EU and 2015/863/EU of the European Parliament. An exemption was granted for lead in copper and brass alloys allowing up to 4% lead by weight.
REACH
REACH is a regulation of the European Union, adopted to improve the protection of human health and the environment from the risks that can be posed by chemicals. As far as the REACH regulation is concerned, LEMO is a producer of items made from finished products. In cooperation with our suppliers and according to our supply channels we are kept informed about their procedures of pre-registration and guarantee the safe use of the items that we supply to you.
Sony Green Partner
The SONY Corporation created the Green Partner Environmental Quality Approval Program as part of its environmental activities in order to maintain and improve the environmental safety and quality of all components and materials that are distributed worldwide in SONY products. Since 2005 LEMO has been awarded by SONY the Green Partner Certificate and we are committed to a continuous cooperation on Sony environmental quality assurance activities.
Proposition 65
Proposition 65 requires businesses to provide warnings to Californians about significant exposures to chemicals that cause cancer, birth defects or other reproductive harm.
Environment FAQ
Find answers to your questions! Explore our FAQ for helpful information dedicated to our Environment section.
什么是 RoHS?
2013 年 1 月 2 日,第 2002/95/EC 号指令被第 2011/65/EU 号指令废止,该指令被称为 RoHS 指令修订版或 RoHS 2 指令。
2015 年,欧盟发布了名为 RoHS 3 的第 2015/863 号指令,扩大了实际指令的范围,增加了 4 种受限物质"。
RoHS 是否有豁免规定?哪些适用于 LEMO?
适用于 LEMO 的豁免:
铅 (Pb):
在钢合金中的含量为 0.35%(豁免 6a - RoHS 附件 III)
铝合金中的 0.4%(豁免 6b--附件 III RoHS)
铜合金中为 4%(豁免 6c--附件 III RoHS)。
LEMO 能否提供 RoHS 的 COC?
什么是 REACH?
LEMO 产品中是否含有 SVHC?
LEMO 致力于在可能的情况下减少或消除这种已确定的 SVHC,并提供足够的信息,以便安全使用该物质。
LEMO 能否提供材料声明?
RoHS 的限制物质有哪些?
什么是最大浓度值 (MCV)?
MCV 值如下 按重量计,铅、汞、六价铬、多溴联苯、多溴联苯醚和邻苯二甲酸盐的最大含量为 0.1%。
镉的最大含量为 0.01%(按重量计)"。
什么是均质材料?
什么是候选清单?
从法律上讲,没有任何规定禁止在产品中使用这些物质,但在收到客户要求后的 45 天内,有义务告知客户该分子的名称和防护方法。
欧洲化学品管理局(ECHA)在其网页上公布了 SVHC 清单: (http://echa.europa.eu/web/guest/candidate-list-table)."
什么是 REACH 第 33 条?
RoHS 和 REACH 的共同点和最重要的区别?
最重要的区别在于
- REACH 法规对各类产品中所有物质的生命周期进行监管。RoHS 仅对电气和电子设备中数量非常有限的物质的使用进行监管。
- 物质含量限制的参考依据: REACH -> 零件重量百分比 / RoHS -> 均质材料重量百分比。
什么是 SONY 认证绿色合作伙伴?
LEMO 承诺遵守 "绿色合作伙伴环境质量认证计划",其中对受控物质进行了说明。该文件(SS-00259)汇集了 REACH 和 RoHS 以及其他各国的国家法规。
根据这一承诺,LEMO 对所有供应商进行定期控制、ICP 测试、审计、自我评估和员工培训等"。

Do you
have a
challenging
project?
No matter how harsh the environment may be, LEMO has a solution ready for you to implement today.
If not, we promise to relentlessly innovate and develop one for you.
Please take a moment to reach out and describe your project, technical specifications and deadlines. We’re standing by and looking forward to hearing from you – and adding your business to our thousands of longstanding satisfied customers, partners and employees – very soon.