The 4th J-Parc Symposium 2024
Japan Proton Accelerator Research Complex

 

2024/10/14 - 2024/10/08
Mito City Civic Center
 1-7-1, Izumicho, Mito-city, Ibarak
Japan 310-0026

https://j-parc.jp/symposium/j-parc2024/index.html

To book a meeting, please contact us by form or by email

 

 

We are pleased to announce that the 4th J-PARC symposium (J-PARC2024) will be held on October 14-18, 2024, in Mito, Japan.

The J-PARC facility started its operation of a neutron beam facility in May 2008, a muon facility in September 2008, a hadron facility in February 2009, and a neutrino facility in April 2009. The output beam power of the accelerators is steadily increasing with the progress of the beam tuning and hardware upgrades. The output beam power of the rapid cycling synchrotron is reaching its design goal, 1 MW, and the main ring synchrotron achieved the operation for the neutrino facility at 500 kW.

According to the symposium theme, "Futures of J-PARC, Futures by J-PARC", we will discuss the achievements from 15 years of J-PARC operation together with the progress in relevant fields around the world. We then will discuss future and upgrade plans of J-PARC and other facilities.

The symposium program consists of plenary, parallel, and poster sessions. The scientific program will cover particle and nuclear physics, material and life science, accelerator science, target and related technologies, and R&D for nuclear transmutation. Public lectures for the general audience and a J-PARC tour are planned as well.