Filter
E.g., 2014-07-29
E.g., 2014-07-29
  • 06/30/2014
    LEMO Acquires Custom Cable Manufacturer Northwire
    Ecublens, Switzerland — LEMO, a Swiss global leader in the design and manufacture of precision custom
    connectors, is pleased to announce that they have acquired Northwire, Inc., (NWI) a US specialty cable manufacturer of wire and multi-conductor cable and retractiles for the medical, aerospace and defense, energy and industrial markets.
     
    “The acquisition of Northwire will enlarge the LEMO offering, providing a complete cable-connector solution to our
    valued customers. I am convinced that by creating synergy between our two companies, we can grow and prosper side-by-side. Together we will be able to provide our customers high-quality complete cable-connector solutions. I am very pleased about this new venture with NWI and look forward to developing new business together. I also take the opportunity to emphasize that the Northwire and LEMO existing structures will remain unaltered. The additional processes that we plan to implement will enable Northwire’s integration into the Group and promote our cooperation and services provided to our mutual customers”, said Alexandre Pesci, CEO and President, LEMO Group.
     
    For further information, please contact :
    Raymond Voillat, Sales & Marketing Director, LEMO rvoillat@lemo.com
    or Serge Buechli, Marketing Manager, LEMO sbuechli@lemo.com
     
     
    See attached for the complete press release:
     
  • 05/27/2014
    New MM connector

    Major trends in connector development over the last few years are miniaturisation and increased contact density. System integrators in various markets, such as automotive, testing and aviation, are looking to increase the number of sensors and data acquisition means. Naturally this requires more connectors and cables in reduced space. 

    LEMO is extending its range of M series connectors with the introduction of the new MM series. The MM series is available with 2, 3 or 4 contacts and is be one of the smallest IP 68 connectors of the LEMO range. With this very small connector, LEMO completes its range of connectors for the automotive / racing market by offering connectors suitable for cable diameters 2 to 27 mm and contact configurations ranging from 2 to 114 contacts. 

  • 05/13/2014
    1400 Eagle PCB libraries now online
    Whether you are a design engineer or an electrical engineer, LEMO now offers for download over 1400 Eagle PCB libraries.
    These libraries reduce the efforts and time of the electronic design engineer during PCB design process. No need anymore to spend time in creating CAD Library for specific parts in a design.
     
    The libraries can be downloaded from the LEMO web part search by selecting Termination Type PCB or directly from the cadsoftusa website
     
     
  • 04/07/2014
    LEMO Demonstrates Connector Solutions at NAB 2014, Booth #C9012

    Rohnert Park, California — LEMO (www.lemo.com), a global leader in the design and manufacture of precision custom connection solutions, continues to serve the broadcast marketplace with their high-quality connection solutions for outside (harsh environments) and studio (indoor-use) applications.  LEMO will be demonstrating their connector solutions in Booth #C9012 during NAB, Las Vegas, April 7-10, 2014.  LEMO’s products include the well established 3K.93C HDTV Connection System (SMPTE compatible), Audio/Video Connectors, Digital Media Converters, Portable Fusion Splicing, Cable Assemblies and Fiber Optic Maintenance, Inspection & Cleaning Tools.

    LEMO will have a live demonstration of the HD Z-Link fiber optic camera link system that provides multi-channel camera-style video and audio connections, and control for studio cameras and camcorders over a single hybrid cable using LEMO’s well established high-quality 3K.93C connectors. The use of high bandwidth fiber optics and the multiplexing of numerous forward and return video, audio, talkback and data channels provide full communication with any camera position.

     

     

     

  • 04/02/2014
    Joseph Electronics Now a Certified Assembler of LEMO's 3K.93C Cable Assemblies

    Joseph Electronics Now a Certified Assembler of LEMO’s Well-Established 3K.93C HDTV Cable Assemblies (SMPTE)

    NILES, Ill. April 1, 2014Joseph Electronics (JE), the premier one-stop shop for the broadcast industry and provider of fiber termination and custom fiber solutions through Joseph Fiber Solutions (JFS), today announced that they have been officially certified by LEMO to build and repair SMPTE 311M fiber optic cable assemblies with the LEMO 3K connectors. The LEMO 3K.93C hybrid connectors have a compact design with two single-mode fiber contacts, two power contacts, and two signal contacts for HD camera interconnection systems. The LEMO 3K.93C is fully ANSI/SMPTE (USA), ARIB (Japan), and EBU (Europe) compliant. Joseph Electronics — and its fiber division, Joseph Fiber Solutions — has achieved the highest level of technical excellence in attaining LEMO-certified SMPTE cable assembler status. 

  • 04/02/2014
    BTX Certified as LEMO Assembler of SMPTE Assemblies

    BTX Certified as LEMO Assembler of SMPTE Assemblies Experts in SMPTE LEMO Assemblies and Repairs

    HAWTHORNE, N.Y. — April 7, 2014 — BTX Technologies, a value-added distributor and manufacturer of interface, integration, and system products, today announced that they have been officially certified by LEMO to build and repair LEMO SMPTE cable assemblies

  • 03/03/2014
    New distributor in Chile / Nuevo acuerdo de distribucion en Chile
    LEMO is proud to annonce a new distributor agreement with Trigital in Chile.
    Trigital has established itself in the Broadcast offering technologies, diagnostics, services and maintenance of Hybrid Fiber Optics. In all its forms and extensions with great succes in Chile and with ample opportunities to offer this service to the rest of South America.
     
    LEMO tiene el placer de anunciar un nuevo acuerdo de distribucion con Trigital en Chile.
    Trigital ha logrado posicionarse en la industria del Broadcast ofreciendo technologias para le correcto diagnostico, servicio y mantencion de cables hibridos de Fibra Optica, en todas sus modalidades y extensiones con gran exite en Chile y con amplias posibilidades de ofrecer este servicio en America del Sur
     
  • 01/28/2014
    LEMO Demonstrates New Products at MD&M West 2014, Booth #1659

     

    Rohnert Park, California, USA — LEMO (www.lemo.com), a global leader in the design and manufacture of precision custom connection solutions, will be demonstrating their latest connection solutions for critical medical applications in Booth #1659 during MDM WEST, Anaheim, CA, February 11-13, 2014.  LEMO’s latest in medical connector products include the NEW REDEL® Single Patient-Use Connectors (disposable) plastic push-pull connectors.

    The REDEL brand of LEMO is a well established plastic connector series specifically in the medical market. LEMO will be demonstrating a few new sizes (26 and 34 pin) of these high-quality self-locking plastic connectors for single patient-use.  LEMO recently announced this new line of specialized single-patient use connectors, ideally designed to ensure quality performance in medical applications, yet can be economical enough to justify single-use.  

  • 09/22/2013
    LEMO Canada is moving to a new location
    LEMO Canada is happy to announce that from the 20th of september 2013, we have moved into new business premises. The new location is idealy located in Richmond Hill, Ontario. 
     
    "We're delighted to be moving into this newer and brighter premises. This new office will give us the ability to set up to better meet our current customers' demands and also gives us flexibility  to meet our future growth plans", says Mario Colacino General Manager at LEMO CANADA INC.
    Please note that the phone and fax numbers have changed. Any existing post sent to the current address will find its way to us just fine.
     
     
    The new adress is: 
    LEMO CANADA INC
    44 East Beaver Creek Road
    Unit 20,
    Richmond Hill, Ontario
    L4B 1G8
     
    Tel: +1-905-889-5678
    Fax: +1-905-889-4970
     
  • 07/15/2013
    LEMO Demonstrates its Lightweight Compact COTS Connector Series at AUVSI 2013

    Rohnert Park, California, August 15, 2013 — LEMO, a global leader in the design and manufacture
    of precision custom connection solutions will be displaying its connector series designed specifically for COTS military,
    robotics, security and aerospace, as well as other harsh environment applications that require robust high-quality
    performance in a lightweight compact size at the AUVSI 2013 show. The LEMO M Series was designed for those that
    require a MIL-38999 type connector but in a much smaller, lightweight and compact package with high contact
    densities, while still monitoring or exceeding performance specifications.
     
    To learn more about LEMO’s M Series and other high quality connectors, please visit the LEMO booth at the
    upcoming AUVSI (Association of Unmanned Vehicle Systems International), August 13-15, 2013, Washington, DC,
    Booth #3450. LEMO will be available with product samples and more specific product details.
     
    Find out more in the complete press release attached below (pdf)
     
     

     

  • 04/08/2013 to 04/11/2013
    LEMO Demonstrates Connector Solutions at NAB 2013, Booth #C9012

    LEMO Demonstrates their High Quality HDTV Connectors, Media Converters and Fiber Field Repair Solutions for Broadcast Customers During NAB 2013

    Rohnert Park, California — LEMO (www.lemo.com), a global leader in the design and manufacture of precision custom connection solutions, will be demonstrating their connection solutions for field (harsh environments) and studio (indoor use) applications in Booth #C9012 during NAB, Las Vegas, April 8-11, 2013.  LEMO’s products include the well established 3K.93C HDTV Connection System (SMPTE compatible), Audio/Video Connectors, Digital Media Converters, Portable Fusion Splicing, Cable Assemblies and Fiber Optic Maintenance, Inspection & Cleaning Tools.

    LEMO will have a live demonstration of the HD Z-Link fiber optic camera link system that provides multi-channel camera-style video and audio connections, and control for studio cameras and camcorders over a single hybrid cable using LEMO’s well established high-quality 3K.93C connectors. The use of high bandwidth fiber optics and the multiplexing of numerous forward and return video, audio, talkback and data channels provide full communication with any camera position.   

    FInd our more in the complete press release attached below (pdf)

  • 02/12/2013 to 02/14/2013
    LEMO USA Demonstrates New Products at MDM WEST, Booth #1861

    Rohnert Park, California — LEMO, a global leader in the design and manufacture of precision custom connection solutions, will be demonstrating their latest connection solutions for critical medical applications in Booth #1861 during MDM WEST, Anaheim, CA, February 12-14, 2013.  LEMO’s medical connector products include the NEW REDEL® Single Patient-Use Connectors (disposable), sterilization/soaker caps, as well as their standard metal and plastic push-pull connectors.  

    The REDEL brand of LEMO is a well established plastic connector series specifically in the medical market. LEMO will be demonstrating a few new sizes (26 and 34 pin) of these high-quality self-locking plastic connectors for single patient-use.  LEMO recently announced this new line of specialized single-patient use connectors, ideally designed to ensure quality performance in medical applications, yet can be economical enough to justify single-use. 

    LEMO will also announce their new aluminum soaker (sterilization) caps for the 2B and 3B Series Connectors. These are covers/caps for the connectors that are put in place prior to cleaning or steam sterilization of the equipment, protecting the connector and the contacts (pins).   The perfect solution for medical cable assembly companies that require  their cable assemblies to undergo many sterilization cycles. 

    To complete the connection solution, LEMO also offers integrated electronics and custom cable assemblies.  LEMO’s experts will be in the booth and available to work with you on your specific applications.  Make sure you stop by and visit LEMO at booth #1861!

  • 02/12/2013
    4 new products from LEMO at BVE

    LEMO will be demonstrating 4 new products at BVE exhibition further building on the package of products to support HD camera link systems.

    A new lightweight Furukawa 6.4mm diameter HD hybrid fibre cable is available, manufactured to SMPTE format including steel central strength member with reduced power conductors, to provide a tough but light camera cable offering weight savings of approximately 45% compared to standard SMPTE fibre camera cables. Maximum operating distance is up to 1km depending on camera system.

    Picture 1. View of fibre and copper wires in Furukawa SMPTE cable

    The latest Redel® T7 connector has been developed to meet the increasing demands of HD triax camera applications with significantly improved performance. Fully compatible and exchangeable with the 1051 Series connector commonly used for triax cameras in Europe, the T7 connector has the additional advantages of better VSWR characteristics and a more secure latching mechanism. Available with either solder or crimp contacts and with a wide range of options to handle the majority of triax cable sizes, the Redel T7 connector is fully sealed to IP68 to cope with all weather conditions.

       Picture 2. New T7 series catalogue

    LEMO also offer a high performance HD Triax 11 cable specially manufactured to LEMO specifications to match the excellent transmission properties of the LEMO range of precision triaxial connectors including the new Redel T7 for HD camera applications, with low attenuation and high level EMC screening properties.  Competitively priced against other HD triax cable, it is ideal for both indoor and outdoor use, giving HD transmission distances up to 30% longer than standard triax cable.

    The cable has a black outer jacket making it less likely to be seen during filming in comparison to red coloured cables, especially in studios, as well as helping to distinguish between standard and HD triax cables. It is also relatively light (for example only 30kg for a 200 metre length) for ease of transportation.

    Complete cable assemblies are available to order including boots and gaiters as required.

    New LEMO HD Z-Link camera-back connects camcorders to SMPTE HD fibre links.  See the new Z-Link  along with highly reliable HD triax & HD fibre push-pull connectors and cable assemblies. LEMO connectors and fibre converters are found wherever you need truly dependable connections, whether for audio, video, datacoms or controls.

    For further information visit LEMO on Stand  B35.

    See our website www.lemobroadcast.co.uk

    Email uksales@lemo.com  or call us on +44 1903 234543.

  • 01/16/2013
    NEW Aluminum Soaker (Sterilization) Caps for LEMO’s B Series Connectors

     

    LEMO is now offering aluminum soaker (sterilization) caps for the 2B and 3B Series Connectors. These are covers/caps for the connectors that are put in place prior to cleaning or steam sterilization of the equipment, protecting the connector and the contacts (pins).
     
    This new product will be demonstrated at: MDM West in february 2013
     
  • 12/18/2012
    2012 W.E.C winners Rebellion Racing visit their sponsors LEMO in Worthing

    On their return home for the winter strip-down and rebuild, Rebellion Racing called in on LEMO UK so that staff could have a chance to view at close hand the car that LEMO sponsors. We were also pleased to receive the Mayor and Mayoress, Council Leader Paul Yallop and Deputy Leader Bryan Turner who is also responsible for regeneration.

     

    Rebellion Racing have had an extremely successful season in 2012 winning the FIA WEC Endurance Trophy for LMP1 Private Teams. Rebellion Racing's Lola-Toyota cars secured six wins from eight races (Spa-Francorchamps, Le Mans, Silverstone, Sao Paulo, Fuji and Shanghai) and six pole positions, though were unable to break the overall results of the Manufacturers cars. However, in the 24 hour Le Mans Rebellion were able to break the stranglehold of the manufacturers coming an overall 4th in the race.
    The Rebellion vehicles were on their way to the premises of Sebah Racing near Horsham for their winter re-build in readiness for the 2013 season, in which they will be entering one car in the American Le Mans Series and one car in the 24 hour Le Mans, with remaining participation in other events yet to be finalised.
    LEMO has a strong link with motor racing, featuring in particular on the latest version of the McLaren Electronics F1 ECU. As well as a number of their F Series connectors continued from the precious F1 ECU system, the new ECU has tree of the new LEMO 5M series with up to 114 contacts in a 30mm diameter connector, thus further assisting weight reduction with improved performance in this highly demanding environment.
  • 11/22/2012
    Action taken against counterfeit product at a recent electronic exhibition

     

    Counterfeiting is becoming more and more of a problem for electronic manufacturers, particularly when passed off as original product, resulting in many instances of warranty problems for manufacturers and users alike. 
     
    At a recent exhibition a number of Asian companies were found to be offering direct copies of LEMO Push-Pull connectors, sometimes exactly copying the LEMO branding, catalogue and part numbers. LEMO took appropriate action and, through a combination of customs (illegal import of counterfeit products) and legal means (breaking copyright) these products were cleared from the relevant stands with penalties being imposed. 
     
    LEMO will continue to take every opportunity to demonstrate to counterfeiters and their importers that action can and will be taken against them. 
  • 11/02/2012
    18000 - 3D CAD drawing references now online

     

    18000 - 3D CAD drawing references now online !

    LEMO started working with traceparts in 2010, since then LEMO has continuously improved their online 3D CAD drawing information. On November 1st 2012, we've added an additional 4000 drawings allowing engineers, draftsmen and CAD users to download drawings from our product part search or from traceparts online.

    With the help of additional 3D models on lemo.com, we can now offer a high added value service to our customers.

    Find out more:

    Part search for advanced users

    LEMO drawings on traceparts online

  • 09/25/2012
    USB Connector for Harsh Environment

    LEMO is Now Offering a USB Connector to its M Series Product Line of Harsh Environment Ratchet-Coupling Connectors 

    Rohnert Park, California,  September 25, 2012 — LEMO, a global leader in the design and manufacture of precision custom connection solutions has added a Rugged Waterproof USB Type A Connector (IP68 when mated) to its family of lightweight ratchet-coupling compact connectors.  This particular connector has been designed for outdoor use including oil/petroleum, automotive, mining, military, marine or any type of application that requires rugged and reliable connections.  The complete product line includes panel mount sockets, plugs, and protective caps.
     
    The M Series is designed specifically for COTS military, security & aerospace, as well as other harsh environment applications that require robust performance in a lightweight compact size.  The LEMO M Series Connector Series offers insert configurations from 2 to 114 contacts and is focused on the design engineer that desires a MIL-38999 type connector but in a much smaller, compact, and lightweight package with higher contact densities. 
     
  • 08/30/2012
    Creation of LEMO CANADA Inc.
    LEMO group is proud to announce the creation of LEMO Canada, Inc, based in the Toronto area. This new LEMO entity has been officially established on August 24th, 2012, through the acquisition of Birde Marketing Inc, official distributor of LEMO products in Canada.
     
    Birde Marketing has successfully represented LEMO products in Canada since 1988, achieving regular and steady sales increase during the past 24 years. The Company currently employs 13 people, based in 4 offices across Canada. Mr Mario Colacino, who has been with Birde Marketing since 1988, has been appointed General Manager of LEMO Canada, Inc. 
     
    The acquisition of Birde Marketing reflects our strategy to expand LEMO's presence in major markets. The creation of LEMO Canada will strengthen LEMO's position in North America and create new opportunities to respond to existing and future customer needs. 
     
     
     
  • 08/15/2012
    雷莫上海成功参加2012慕尼黑电子展

    慕尼黑上海电子展(electronica & Productronica China 2012)于2012年3月20至22日在上海新国际博览中心召开。今年的展会是慕尼黑电子展在上海的第十一届展会,也是雷莫第七次参展。 今年展会现场突破性地有来自19个国家与地区的664家展商,向41,847名专业观众展示了最新的产品与热门应用领域的解决方案。继2007、2011年雷莫申请了36平米参展以后,今年,雷莫申请了54平米的大展位。并在展台搭建了表演舞台,邀请了吉他演奏和行为艺术来吸引现场观众的眼球,大展位和精致的布置也给我们带来了巨大的曝光量,一步入展馆,马上就能看到雷莫的Logo和标识,而现场的表演让观众们驻足观看、拍摄,使得雷莫在整个展馆内大放光彩。

     

  • 05/22/2012
    NEW REDEL Brand of Single Patient-Use Connectors

    LEMO Demonstrates the NEW REDEL Brand of Single Patient-Use Connectors at MDM EAST 2012

    Rohnert Park, California – LEMO (www.lemo.com), a global leader in the design and manufacture of precision custom connection solutions, will be demonstrating their latest connection solutions for critical medical
    applications in Booth #1562 during MDM EAST, Philadelphia, PA, May 22-24, 2012. LEMO’s medical connector products include the NEW REDEL® Single Patient-Use Connectors, the REDEL XP Series as well as their standard
    metal push-pull connectors.

    The REDEL brand of LEMO connectors is a well established product series in the medical market and LEMO understands the importance of sterilization in minimally invasive electro-surgical procedures. These are high-quality
    self-locking plastic connectors offering sterilizable connector / cable solutions and single patient-use connector solutions. LEMO has recently announced a new line of specialized single-patient use connectors that are ideally
    designed to ensure quality performance in medical applications, yet can be economical enough to justify single-use.
    The REDEL® XP connector is designed using a plastic material that is friendly to sterilization processes. The latching system is embedded in the shell for an increased impact resistance with a high contact density making this an
    ideal solution for medical or measurement applications, from catheters to surgical instruments. To complete the connection solution, LEMO also offers integrated electronics and custom cable assemblies.
    LEMO’s experts will be in the booth and available to work with you on your specific applications. 

    Find out more in the complete press release (pdf)

  • 04/16/2012
    LEMO at NAB 2012 demonstrates
    Rohnert Park, California – LEMO (www.lemo.com), a global leader in the design and manufacture of precision custom connection solutions, will be demonstrating the latest connection solutions for field (harsh environments) and studio (indoor use) applications in Booth #C9012 during NAB, Las Vegas, April 16-19, 2012.
     
    LEMO’s products include the well established 3K.93C HDTV Connection System (SMPTE compatible), Audio/Video Connectors, Digital Media Converters, Portable Fusion Splicing, Cable Assemblies and Fiber Optic Maintenance, Inspection & Cleaning Tools.
    LEMO will be demonstrating the HD Z-Link fiber optic camera link system that provides multichannel system camera-style video and audio connections, and control for studio cameras and camcorders alike over a single hybrid cable using the LEMO 3K.93C connectors. The use of high bandwidth fiber optics and the multiplexing of numerous forward and return video, audio, talkback and data channels provide full communication with any camera position.
  • 01/26/2012
    Digikey distribution agreement
    Digi-Key Corporation Signs Global Distribution Agreement with LEMO
     
    THIEF RIVER FALLS, Minn., USA – Electronic components distributor Digi-Key Corporation, recognized by design engineers as having the industry’s largest selection of electronic components available for immediate shipment, and LEMO®, a global leader in the design and manufacture of precision custom connection solutions, today announced the companies have signed an agreement in which Digi-Key will be LEMO’s first global distributor.
     
    “Engineers are continually faced with the need for connectors to meet the challenges presented in a variety of applications,” said Jeff Shafer, Digi-Key’s vice president of interconnect, passive, and electromechanical products. “LEMO is a leader in meeting this demand with the design and manufacture of their push-pull connectors and we are pleased to offer their products to our global customers.”
     
    “LEMO strives to achieve the highest level of quality and customer satisfaction,” said Dean Pohwala, general manager, LEMO USA, Inc. “With the addition of Digi-Key, we can now offer customers extended customer service delivered with technical expertise, professionalism and speed. We are very happy to have Digi-Key as part of our distribution network and we look forward to a very successful partnership.”
     
  • 01/09/2012
    New General Manager at LEMO USA Inc.
    ROHNERT PARK, Calif., January 9, 2012 – LEMO USA, Inc., subsidiary of LEMO SA,
    Switzerland, (www.lemo.com), and a global leader in the design and manufacture of precision custom connection solutions, announced today the appointment of Dean Pohwala as the new General Manager, nominated by the President of the Board, Alexandre Pesci.
    Dean will replace Albert Meylan, who has been the acting GM since October 2010. Albert will be returning to another management position at LEMO Headquarters in Switzerland.
    Since March of 2011, Dean held the National Sales Manager position where he drove the development and implementation of the sales business plan and provided guidance to the North American sales reps and distributor network.
     
  • 10/11/2011
    3D drawings on tracepartsonline.net
    Ecublens, Switzerland Oct 11, 2010 
     
    LEMO S.A has added an entire range of 3D drawings on tracepartsonline.net. Traceparts is one of the biggest parts libraries in the world, offering 100 million free 2D drawings & 3D CAD models
     
    Now up to 10'000 LEMO CAD drawings can be downloaded online from traceparts. Models include the B,K,S,E series, as well as F series and the M series for the military market. Medical REDEL P series connector can also be viewed and downloaded online making it easier than ever for CAD users to turn their 3D designs into reality. 
     
    Available formats are: 
    • 2D formats: DXF (7 views), DWG (7 views), Images (TIFF, GIF, JPEG, PNG, WMF, etc.)
    • 3D neutral formats: DXF, DWG, IGES, STEP, ACIS, PARASOLID
    • 3D native formats: CATIA, Inventor, Pro/Engineer, Mechanical desktop, Solid Edge, TopSolid, thinkdesign, Unigraphics, Solidworks, Topsolid, Google SketchUp, TurboCAD, Alibre Design, 3D XML...
     

     

  • 08/26/2011
    New HD Z-link at IBC 2011
    LEMO is looking forward to welcoming you this year at IBC 2011 to our booth in Hall 11.C45. LEMO will be showing it's entire range of broadcast converters including the innovative new HD Z-link as well as our traditional range of triax and LEMO's 3K.93C series. 
     
    LEMO will be demonstrating a new product, the HD Z-Link fiber optic camera link system that provides multi-channel system camera-style video and audio connections, and control for studio ca eras and camcorders alike over a single hybrid cable using the LEMO 3K.93C connectors. The use of high bandwidth fiber optics and the multiplexing of numerous forward and return video, audio, talkback and data channels provide full communication with any camera position. 
     
    The dual 1.5Gb/s HD SDI option allows support of stereoscopic (3D) implementations of the Red One ® (and other cameras). The HD Z-Link is able to carry 3Gb/s HD SDI which gives it a competitive advantage over the 2.5Gb/s products that do not support 1080P.
     
     
  • 08/07/2011
    LEMO Demonstrates its Lightweight Compact COTS Connector Series

    LEMO Demonstrates its Lightweight Compact COTS Connector Series Designed for Military, Security, Aerospace and Automotive during AUVSI 2012

    Rohnert Park, California, August 7, 2012 – LEMO, a global leader in the design and manufacture of precision custom connection solutions will be displaying its new connector series designed specifically for COTS military, security & aerospace, as well as other harsh environment applications that require robust performance in a lightweight compact size. The LEMO M Series Connector family offers insert configurations from 2 to 114 contacts and this product is focused on the design engineer that desires a MIL-38999 type connector but in a much smaller, compact and lightweight package with higher contact densities.
     
  • 05/01/2011
    New factory in Budapest Hungary

    Ecublens, Switzerland 

    To increase LEMO's production capacities, a new factory has been built in Budapest-Hungary. The new factory has been running since November 2010 and has a total surface of 10'240 m2, it's the only factory in the LEMO group that combines all the manufacturing process within one site, injection molding, assembly and plating....
     
     LEMO continues to produce its main volume in Sainte-Croix and Delémont Switzerland
     
     
     
  • 01/10/2011
    Back to the future - the return of LEMO UK
    Worthing, UK 
    Back to the future–the return of LEMO UK to new headquarters and a new website.
    After a 4 year absence LEMO UK have returned to their North Street location in Worthing to a new, multi-million pound, futuristic building that provides the space and modern facilities to continue our development as a supplier of high quality interconnection solutions for niche applications in industries such as Broadcast, Defence, Scientific Research and Test and Measurement.
     
    LEMO UK occupied 12 North Street for 17 years prior to moving out to temporary premises nearby, acquiring the Caffyns site next door to provide the space for our 3,700 sq m modern and stylish building that now adds a new dimension to Worthing's skyline. The new facilities will house all our UK operations including Engineering, Manufacturing, Distribution, Administration and Sales & Marketing, as well as the LEMO Group's Fibre Optic R&D centre - LEMO F.O.U.R.
     
    The basement of the building will house our extensive cable stock and cable reeling equipment, connector stores and assembly will be on the ground floor along with our prototyping machine shop. The first floor will house our sales, technical and production administration, our large and light cable assembly and test shop and the Fibre Optics R&D engineering, laboratory and training centre. General administration, accounts and our conference room are on the second floor, but there is also additional space on this level for expansion of manufacturing when required. There is a cafe on the 3rd floor where employees can relax and enjoy the views of the Worthing skyline and the picturesque South Downs to the north. 
  • 11/03/2010
    New REDEL XP at Electronica
    With the new REDEL® XP, LEMO is introducing a revolutionary patented solution of the plastic Push-Pull connector. The latching system is now embedded in the shell, offering an increased impact resistance and a very high contact density. 
     
    The REDEL® XP offers multiple contact and colour configurations and suits a wide array of medical or measurement applications, from catheters to surgical instruments. 
     
    Decades of know-how and experience have allowed LEMO to launch the new high performance REDEL® XP connector. Made of Sulfone proprietary material, the connector is very resistant to sterilisation such as autoclave, making it ideal for medical applications. 
     
    The product is available in a large choice of colour codings; black, white, grey, green, blue, yellow, red. Contact configurations range from 4 to 22 contact and can be crimp or solder type. The outershell is available in grey, black or white colour, it’s easy grip design makes it much easier for surgeons and medical staff to hold and use. 
     
    The flexibility of its design allows any manufacturer of electrical devices to keep a minimum stock of sub-components that can generate a large range of final connector assemblies. 
     
     
     
     
  • 09/03/2010
    Nuevo REDEL 1P con cuerpo exterior metálico
    El nuevo conector REDEL 1P con cuerpo exterior metálico ofrece nuevas oportunidades para los sistemas de interconexión. Además de las aplicaciones médicas, el REDEL 1P se utiliza cada vez más en aplicaciones de I+D e Instrumentación.
    El cuerpo exterior metálico se fábrica con aluminio ecológico (con acabado gris).
    El cuerpo exterior metálico hace de esta versión el conector más robusto, mientras que los conectores machos siguen siendo perfectamente compatibles con las hembras de panel REDEL 1P actuales.
     
  • 09/03/2010
    New REDEL 1P with a metallic shell
    The new REDEL 1P with a metallic outershell offers new opportunities for interconnection systems. Aside from the medical applications, the REDEL 1P is used more and more in measurement and instrumentation applications.
     
    The metallic outershell is made of ecological aluminium (grey finish). The metallic shell makes this version of the connector more robust, while the plugs remain perfectly compatible with the actual REDEL 1P sockets (receptacles).
     
  • 07/06/2010
    High voltage connector for avionics
    LEMO S.A is pleased to announce the launch of its new high voltage connector for avionics. 
     
    The connector’s design prevents voltage creeping on the surface of the insulator.
    LEMO’s high altitude connector will operate correctly during pressure drop and temperature cycle. Test voltage >30 kV @ 70'000ft. The HY series is made of PEEK outershell and is designed to be used only with a non shielded cable. 
     
  • 01/05/2010
    Opening of LEMO Asia Ltd, Singapore

     

    Ecublens, Switzerland

    January 2010 sees the opening of LEMO Asia Ltd, in Singapore. Drawing on our success & expertise, this latest facility will allow customers in Singapore, Malaysia, Philippines, Thailand, Indonesia, Vietnam and south east asia in general to receive customer service such as technical support, design facilities and customer sales services. 

     

    Contact information:
    LEMO Asia Pte Ltd
    4 Leng Kee Road, #06-09 SiS Building
    159088 Singapore
    Tel: 65 6476 0672
    Fax: 65 6474 0672
    email: sg.sales@lemo.com

  • 01/04/2010
    LEMO relies on Autodesk software

    Rohnert Park, United States 

    Running concepts by customers without having to create physical prototypes is one of the most valuable benefits we get from Digital Prototyping. Not only can we develop products faster, we have increased the pace of innovation.
     
  • 09/08/2009
    REDEL 1P now also in white colour
    REDEL 1P now also in white colour ! Designed for the medical sector, the REDEL 1P connector is available in grey, black and white colour.
     
    Benefits:
    • lightweight
    • EtO and gamma sterilisable
    • wide choice of colours for easy identification
      (grey, blue, yellow, black, red, green and white)
     
    Feature:
    • available in 2 to 14 contacts
    • outershell in PSU
    • golden contacts
     
  • 02/10/2009
    LEMO acquire Z-link

    September 2008 - LEMO has acquired a product called Z-Link from Cove-Broadcast , this is a fibre optic camera link system allowing transformation of a professional camera or camcorder into a TV live production camera.

    LEMO presented the Z-link at IBC 2008 exhibition (Amsterdam). The Z-Link is a versatile camera-mounted fibre optic camera link between any professional camera or camcorder and an OB Van, studio or outside broadcast place. This means that an ENG camera can be simply and quickly modified for studio or remote camera use if required. The Z-Link is a cost effective alternative solution for expensive studio cameras.
     
    The Z-Link provides multi-channel system camera-style video and audio connections, and control for studio cameras and camcorders alike. The fibre optic camera link simultaneously transmits digital (SDI) and analogue channel (YPrPb and PAL/NTSC), all over one thin light cable.
     
    Applications:
    • Electronic News Gathering / Satellite News Gathering (ENG/SNG)
    • Electronic Field Production (EFP)
    • Outside Broadcast (OB)
    • Live News, Multi-camera, E-Cinema production
  • 01/26/2006
    RoHS

    LEMO Connectors and Accessories

    LEMO certifies that connectors produced and marketed by LEMO S.A. Ecublens, Switzerland, under the brands LEMO, REDEL and COELVER are free of: mercury, cadmium, lead, hexavalent chromium, polybromide biphenyl (PBB) or polybromide diphenyl ether (PBDE), including DecaBDE, according to the requirements of the Directive 2002/95/EC of the European Parliament and of the Council dated 27th January 2003.
     
    This does not apply yet to our connectors with aluminum shell. LEMO plans to achieve full conformity no later than first quarter of 2006.